![]() |
|
Here you will find tips for working with the Schmersal Website. If you should meet any problems with it or if you wish to make suggestions for improvements, please send an E-mail to: info@schmersal.de. Technical requirementsOur site is optimised for web browsers such as Internet Explorer from Generation 4.0 and Netscape Navigator from Generation 4.5. The layout requires screen definition of at least 800 x 600 pixel. For the best picture, 1024 x 768 pixel should be used. Acrobat ReaderIn order to make the original pages of the printed version accessible, we offer you some documents on our website in PDF format. For these documents, the Adobe Acrobat Reader is needed. Navigation on the websiteThere are two ways of navigation: Either via the upper menu strip, from where press information or jobs on offer can be reached directly, for example, or via the vertical menu strip on the left-hand side of the screen, from which detailed information on the company and its products can be obtained. The Online Catalogue is also accessible here. PrintingYou can print many of the documents. The printing details are already optimised for paper size DIN A4. |