Safety in system: Protection for man and machine - under this motto, the Schmersal Group develops and produces safety switching appliances and systems for the entire machinery and plant construction for decennia already. In some industries, special and additional requirements are applicable.
As customer-focussed company, who intensively deals with the wishes of the manufacturer and users of machines, Schmersal has taken up these challenges from the start. As a result, specific products and solutions were developped for many industries and for some of them, an own portfolio has been developped as well.
Harvesting, drying, filleting, heating, shredding and crushing, mixing, filling, packing: The food-processing industry includes many, usually mechanically performed process steps. During these process steps, the standards and directives with regard to machinery safety must be observed. Moreover, the food-processing industry in particular has other fields of activity as well, where the selection of switchgear or command devices at the manmachine interface is highly important.
Hygiene is a key issue in the food-processing industry. Four hygienic zones can be distinguished, for which strictly defined constructive details of the "hygienic design" are applicable:
The Hygienic Design also influences the choice of safety switchgear. An example: the food-processing industry was the first branch, which used safety sensors instead of the conventional electromechanical safety switches. These non-contact operating safety switchgear can be smoothly cleaned due to the smooth surfaces of the sensor and the actuator and moreover provide for concealed mounting.
Stringent hygienic standards are applicable to those components or periphery of foodprocessing machinery, which are in contact with the product; as a result, the safety switchgear and actuating elements must meet the highest requirements as their protection class is regarded. Many series therefore are IP69K. These switchgear must be able withstanding a water jet of at least 80 bar with a temperature of 80°C.
In frozen storage or in case of shock freezing - to name two examples - automated processes take place at temperatures below the freezing point. Even more frequent are the processes, for which high temperatures are inevitable, e.g. evaporation, homogenisation, drying, condensation, distillation. Switchgear, which are used for these processes, must be accordingly highand low-temperature resistent.
The specific characteristics to be featured by machinery and plants destined to the foodprocessing industry are laid down in different regulations, which also concern the individual machinery and plant components and which are in part very demanding. This includes, amongst others, the following standards and approvals according to the following standards:
Switchgear from Schmersal is approved and certified in accordance with these regulations depending on the requirements.
In food production, machinery and plants often operate with short cycles and in a three-shift operation in interlinked plants. The expected availability is accordingly high. Schmersal switchgear meet these requirements. They stand the test in various applications, even under unfavorable ambient conditions.
When mixed to air in a particular proportion, all organic dusts are inflammable. Therefore, the regulations of the dust explosion directive must be observed e.g. when filling/bottling and storing powdered food products and their primary products (flour, baking mixtures, pudding powder, coffee and cacao powder). The Schmersal Group offers a comprehensive range of switchgear for automation and machine safety, which is approved and certified to the ATEX and IECEx Directives.
The Schmersal Group furthermore aims at establishing good contacts and exchanging experiences with food-processing machinery builders, so that new switchgear is developped and the individual consultancy is provided with the highest level of practice-orientation. T o that effect, Schmersal is, amongst others, member of the "Packaging Excellence Center" (PEC). This Centre of Competence for packaging and automation technology reunites many companies manufacturing machinery and plants for the food packaging industry.
The HYGIENEFENCE fence system is an economical safety fence system, which meets the especially high requirements and the legal safety and quality prescriptions, which are applicable in the food-processing industry.
High-grade stainless steel guarantees cleanliness and long lifetime. A HACCP/GMP-compliant design with water- and dirt-resistant construction enables cleaning without traces and residues. The long lifetime, the smooth maintenance and the robustness of the protective device guarantee an ecomical price/performance ratio.
Packaging industry
VDMA Association
Newsletter Issue 2011/02
Hygiene at the man-machine interface. Ergonomics on meat-processing machinery more
In the spotlight: machine safety in food production and processing more
POLAGRA-FOOD, Posen (Poland)
(12. - 15. September 2011)
more
ANUGA, Cologne (Germany)
(08. - 12. Oktober)
more
Cibustec, Parma (Italy)
(18. - 21. October 2011 (hall 6, both A052)
mehr
Brochure "Food industry"(pdf, 5,5 MB)
Office
Manuela Kamusella-Schultz
+49-(0)64 1-98 48 00
E-mail: info-elan@schmersal.com
Industry Manager
Friedhelm Pietzsch
+49-(0)64 1-98 48 412
E-mail: food@schmersal.com