You are here

Content

16.12.2016

Schmersal Safety Control with new address

The business with optoelectronic security products is growing and thriving - and since Safety Control GmbH, which is part of the Schmersal Group, is on an expansion course, it has now obtained a larger building.
The address is now as follows: Am Industriepark 2a, 84453 Mühldorf / Inn, Germany, this is near the old site.
In the new domicile, all activities which were previously split between two buildings are now combined under one roof. It is a three-storey building covering 2,000 m² dealing with logistics and production and an overall area of approx. 3,800 m². “The new building covers our increasing need for production space and offers us the opportunity for further growth,” says director Klaus Schuster.
The contact partners at Safety Control are also available on the usual contact details and telephone numbers.

 

 

Context Column