To Top
The new BDF20 control panel from Schmersal
As a stand-alone solution or system module
New Doorhandle System DHS
Ergonomic Design. Particularly suitable for profile systems.
new versionof SD Gateway
Enhanced productivity with high-performance error diagnosissis
EX-SLC/SLG440 Safety light curtains/grids in Ex design
The H series Hygienic command and signalling devices

4D models of safety-related components

Digital twin for the virtual commissioning of machines and systems

Schmersal is expanding its digital portfolio to include realistic 4D models of safety-related components, opening up new perspectives for virtual machine planning. These include the digital twin of the AZM40 solenoid interlock, the DHS door handle system and the BDF40 control panel.

These 4D models not only depict the geometric properties of the physical components in three dimensions, but also add a fourth dimension: the behaviour in real operation.

Components such as the AZM40 solenoid interlock are reproduced completely digitally and behave exactly like their real-life counterparts in virtual space. The virtual mapping of signal currents and control sequences allows complete machine processes to be simulated realistically.

4D models of safety-related components

A key advantage of 4D models is the ability to commission machines and systems virtually - even before they are physically installed. This allows errors to be detected at an early stage, optimises development processes and saves costs. The possibility of connecting 4D models directly to real control systems, for example via Beckhoff or Siemens systems, is particularly noteworthy. In this way, system settings and control programs can be tested and optimised before actual commissioning takes place.

Standardised simulation: Schmersal relies on FMU models

One innovation is the availability of behavioural models as FMUs (Functional Mock-up Units). This enables standardised integration into different simulation environments such as Siemens Simit, the 3DEXPERIENCE platform from 3DS or ISG-virtuos. 

This significantly improves the interchangeability and reusability of the models – a decisive step for the scalability of digital twins in the industry.

Interested in FMU models?
The simulation models are available on request. Please contact Schmersal for further details and project-specific support:

 

Christoph Rosebrock
Concept Developer Data Analyst
crosebrock@dont-want-spam.schmersal.com

Volker Heinzer
Strategic Product Manager
vheinzer@dont-want-spam.schmersal.com

AZM40 opens digital model catalogue in TwinStore

The 4D model of the AZM40 was also the first Schmersal component to be published and made available in the "TwinStore" – an online store for prefabricated and ready-to-use 4D simulation models. 

The release of the AZM40 as the first TwinStore package marks the start of a successive expansion of the Schmersal Group's digital model catalogue.

Cookies / Privacy Policy
We respect your privacy
This website uses cookies. Further information on the cookies used can be found in our data protection declaration. By clicking on the "Accept all" button, you consent to the use of all of these cookies. By clicking the "Accept selected" button, you only consent to the use of cookies for the purposes you have selected.
Your choice: